Part Number: PCM5102 Other Parts Discussed in Thread: PCM5142 Can you kindly explain the DEMP pin 10 more fully?
If enabled, is it enabled continuously, or only when the emphasis bit 5 is set in the I2S stream?
If disabled, it's killed completely regardless…
Part Number: PCM5100A Other Parts Discussed in Thread: PCM5102 , PCM5100
Hi team,
My customer is facing supply situation on PCM5100APWR.
Could you please check if PCM5100APWR can be replaced by PCM5102PWR? And are PCM510xA and PCM510x devices only different…
Part Number: PCM5102A Other Parts Discussed in Thread: PCM5102 , Hi TI team,
PCM5102 is NRND.
What is the difference between PCM5102 and PCM5102A?
Thanks
Downey Kim.
Part Number: PCM5102A-Q1 Other Parts Discussed in Thread: PCM5102 Hi expert,
In the layout of PCM5102, can I seperate AGND and DGND into two different GND? May be its better to reduce noise from DVDD?
Part Number: PCM5102EVM-U Hello experts,
due to unavailability of supporter from Germany, I need help for further help.
please find attached file of detailed description.
RE PCM5102 IC - Discussion.msg
please help further to solve issue.
Regard, Moh…
Hello Sujisha,
I found PCM5122 EVM and I verified it in HW mode -without any need to program it , the part was able to function for various non-audio freq that I applied through the AP2700 series . I tried freq up to 216K, since AP2700 can not go above fs…
Part Number: PCM5102 Hello,
This is a rather silly question, but when driving IO pins such as XSMT, FLT, DEMP, and FMT is it required that I place a resistor between the pin and the GND / +3.3v? I've assembled a test board and it's not functional, so…
Hello Mohit,
I went to lab and tested The EVM on my bench first with SCLK and then simply removed it from the EVM . The DAC was still functioning -without any need to do any modification. I used AP2700 to generate the 3 wire I2S with 1KHZ sinewave input…
Part Number: PCM5102 Other Parts Discussed in Thread: PCM5122 , PCM5142
Hi, Team
My automotive customer is using PCM5102A in their car infotainment system. They find that there is pop noise when end-user pause and play music in the music player. Is there…
Part Number: PCM5102-Q1 Other Parts Discussed in Thread: PCM1753-Q1 , PCM1789-Q1 Dear all,
one of my AA, would use the sample rate fs=20.5KHz, but this is not allowed in neither 3-wire and 4-wire mode.
Is there any other Automotive Audio DAC which supports…