Part Number: PCM5102EVM-U Other Parts Discussed in Thread: PCM5102 , PCM5102A ,
Hi team,
My customer has a problem connecting PCM5102EVM to Windows 11.
Device recognized as "USB-miniEVM" on Windows 11
CodecControl shows "Communication error…
Part Number: PCM5102EVM-U Other Parts Discussed in Thread: SRC4392 Tool/software: Hello.
PCM5102EVM-U is used for evaluation. I want to write 0x011 to the SRC4392 register (SRCIS[1:0]) after connecting to a PC via USB and launching CodecControl. Is…
Part Number: PCM5102EVM-U Tool/software: Hello Expert,
This EVM's layer 2 and 3 seems there isn't beta GND at analog side. Is there any reason of this design especially relating noise?
We observed huge noise which is synchronized with CAPP/CAPM…
Part Number: PCM5102EVM-U Hello experts,
due to unavailability of supporter from Germany, I need help for further help.
please find attached file of detailed description.
RE PCM5102 IC - Discussion.msg
please help further to solve issue.
…
Part Number: PCM5102EVM-U Other Parts Discussed in Thread: PCM5121 , PCM5100 Hi
We are now evaluate PCM5102EVM-U, our setup as below
1. remove all jumper from W3
2. I2S signal feed to W3 pin 20, 22, 24, and 26 with
SCK = 5.6MHz
BCK = 2.8MHz…
Part Number: PCM5102EVM-U
Hello exprets,
I want to use 3-wire I2S with PCM5102EVM board.
I am giving power to board through USB cable and 3 signals are connected at right side (analoge side). I want to validate my connection because IC is not giving…
Part Number: PCM5102EVM-U Hi team,
I'm trying to connect an external I2S source to PCM5102EVM-U. To do that I removed all the jumpers on W3.
Then connected jumpers as below.
FLT: GND(normal latency)
SCK: GND to use internal PLL
BCK: external…
Part Number: PCM5102EVM-U Other Parts Discussed in Thread: PCM5142 , PUREPATHCONSOLE , PCM1862EVM , PCM5102A , PCM5102 , PCM1862 The Software I downloaded from the web (slac493a) is not for PCM5102EVM-U , but for: PCM5101EVM-S (see attached image) . …
Part Number: PCM5102EVM-U Other Parts Discussed in Thread: PCM5142 Hello,
I would like to ask you about EVM usage.
Is there any tool to generate input date to EVM?
If no tool, how to generate the data.
Thanks and best regards,
Katsu