Part Number: PCM5121 Hi team,
For hardware master mode, where the BCLK and the LRCLK are supplied by the PCM512x chipset,
How does the PCM512x knows what fs is to clock out by the LRCLK since there are several choices .
For example: when sck is supplied…
Part Number: PCM5121 Hi Team,,
My customer is currently looking at using TI Audio DAC for their project.
They are currently looking at PCM5121. Please see the below enquiry:
Pin 14 can be use to choose between I2S Master or I2S slave, and pin 24 can be…
Part Number: PCM5121 The temperature information of the PCM5121 is a little confusing. Here Information of datasheet:
Here the information of product web site:
Can the PCM5121 be used in an industrial temperature range with an ambient -40..85 °C…
Part Number: PCM5121 Other Parts Discussed in Thread: PUREPATHSTUDIO Hello Experts, My customer is considering to use PCM5121 by a following conditions. 1. Software mode 2. PLL will use 3. SCK does not input. SCK will create from BCK. 4. mini DSP(fixed function…
Part Number: PCM5121 Hi Team,
when I test the PCM5121EVM the delay time is not match with the datasheet descprition.
in datasheet the 0x02 preset flow delay time is 3.5/fs, when fs=48K, but the AP actual test DUT delay time result is 104.3us.
the 0x07…
Part Number: PCM5121 Hi Team,
I want to disable the Auto mute. I have red the data sheet of PCM5121. However, there seems to be mistakes in the attached table section below. Please let me know for clarification. To disable the Auto mute, should I send 0x04…
Part Number: PCM5121 Other Parts Discussed in Thread: PCM1690 , PCM1681 HI, Team
Customer prefer to use 2 pcs PCM5121 for 4 channel DAC, and they prefer use the same TDM interface for 2 PCM5121.
I suppose our device can't support that, do u have any suggestions…
Part Number: PCM5121 It is not output from PCM5121.
I'm trying to output from the OUTL pin with a single end, but the voltage is still 0V.
Please tell me the possible causes and what to check.
I have confirmed the following.
-3.3V is supplied…