Part Number: PCM5122EVM-U Hello,
My customer will use PCM5122EVM-U with CodecControl,but we cannot find this software. Could you please provide related links?
Best Regards, itabi
Part Number: PCM5122EVM-U Other Parts Discussed in Thread: PCM5121 , , PCM5142EVM-U Dear Sirs,
I have a question.
I will using PCM5121.
But there is not PCM5121EVM. There is PCM5122EVM-U.
So I checked useguide for PCM5122EVM-U and PCM5142EVM-U…
Other Parts Discussed in Thread: PCM5122EVM-U , PCM5122 Hello, I am trying to get the a PCM5122EVM-U board working. So far, I have gotten the driver installed and working on my PC. I was able to load the "USB-AudioEVM0354_441KHZ.BIN" file onto the board…
Part Number: PCM5122EVM-U Other Parts Discussed in Thread: PCM5122 Hi,
I just recently got the PCM5122 EVM board. I connected the board to my laptop (The driver is automatically installed). I opened some music files but I can not hear anything coming…
Part Number: PCM5122EVM-U Other Parts Discussed in Thread: PUREPATHCONSOLE , PCM5142 , PCM5122 When trying to connect via PurePath Studio I get
Connecting to the EVM. Found board type: FWIDPCM5101EVM-S. Board sampling rate: 48000Hz. Application run…
Other Parts Discussed in Thread: PCM5122EVM-U
Hi,
I followed the directions below to connect the PCM5122EVM-U to my computer through the USB port. I met some problems.
1. Why should I short the SDA and SCL together? or do I need to disconnect…
Other Parts Discussed in Thread: PCM5122EVM-U , PCM5122 Hi,
Our customer would like to know about PCM5122EVM-U well but it's not available in TI's HP.
Can you please provide it?
Best Regards,
Sonoki
Other Parts Discussed in Thread: PCM5122 , SRC4392 Hi
I am testing a PCM5122 using the Evaluation board and feeding 192kHz SPDIF audio into the Coax input and monitoring the Output on a Prism Sound Dscope Audio analyser.
The SRC on the Evaluation…
Arash,
We purchased the eval board PCM5122EVM-U as a reference.
We are having difficulty even getting the Eval board to be recognized by Windows 11.
We downloaded the CC PCM5101 Demo software (supposed to be compatable with the PCM5122)
When we…
I don't think it needs any specific firmware , I know if you use the EVM, then you need to download the latest TAS1020 USB firmware from the PCM5122EVM-U or PCM5142EVM-U product pages.