Part Number: PCM5252 Hi,
As before, I am trying to use Spartan-6 as master and DAC PCM5252 as a host. As it was suggested before, I am SPI mode to program the registers, 4-wire I2S interface, 32 bits, Flrck = 96kHz, Fbck = 64 * Fs, Fsck = 128*Fs.…
Other Parts Discussed in Thread: PCM5252 , PCM5242 , PCM3070 Hello,
We are looking for a 1.1 configuration and are in the process of choosing an AMP for the same. We were suggested PCM5252 as it has excursion control. However, we figured that one of…
Part Number: PCM5122 Other Parts Discussed in Thread: TAD5112-Q1 , TAD5212-Q1 , TAD5112 , TAD5212 , PCM5252 , PCM5242 , PCM5102A-Q1 , PCM5102A , PCM5142
Hi,
To get better audio performance, we want to replace PCM5122 used in XMOS official EVM xk-audio…
Part Number: PCM5242 Other Parts Discussed in Thread: PCM5252 Tool/software: Dear TI Support Team,
I am currently working with the PCM5242/PCM5252 and using PurePath Studio to design the MiniDSP configuration. I have successfully loaded the program…
Part Number: TIDA-01414 Other Parts Discussed in Thread: PCM5252 Dear TI Team,
I want to connect the HDMI eARC receiver connector to this design TIDA-01414. The digital input header consists of (clock, word select, serial data) signals on its input…
Part Number: TIDA-01414 Other Parts Discussed in Thread: PCM9211 , PCM5252 , DIX9211
Dear TI Team,
I am an electronics engineer used TI reference kits during my studies and currently in my professional life. Moreover, currently, I am working on the…
Hi,
For now it is fixed to +/-15V, but if it is goint to be changed, it would be bigger tha +-15V,
I watched that 32 bits DAC PCM5252, it has max sample rate 384KHz , it would work for the signal of 160Hz( more exactly 152.2Hz), but for the a signal…
From reading datasheet , I too don't think it is capable of doing so . I also found this post and I quote from it:
"TI does not have a dedicated device for this function. I believe we have some DSPs that would be able to do this (C6000), but to my knowledge…
Part Number: PCM5242 Other Parts Discussed in Thread: PCM1795 , PCM5252 , PCM1792A Hi,
In examining the performance of the latest DAC IC’s, despite TI offering DAC’s with 32bit capability, the performance of the latest IC’s (PCM5242, PCM5252) is significantly…
Hi Andy,
At this point the devices we are most interested in are as follows:
PCM5252
PCM3070
TLV320ADC3101
but also PCM1804, but this has no miniDSP (shame)
As a matter of interest the PCM5252 are actually driving TPA3255. This TPA3255 is…