Part Number: PCM6020-Q1 Hi team,
How much should I wait after releasing SHDNZ of PCM6020-Q1?
There are 2 description in the datasheet which mention slightly different number. 1ms vs 2ms.
In the datasheet Page 119
"2. Transition from hardware shutdown…
Part Number: PCM6020-Q1 Hi team,
Could you confirm if my understanding below correct?
What is the BSTOUT voltage? --> 1V above set MICBIAS voltage.
How much is the BSTOUOT switching frequency --> 6.144MHz (at fs=48kHz) or 5.6MHz(at fs=44.1kHz) …
Part Number: PCM6020-Q1 Hi team,
I found the default value of following resistor is different from the default datasheet value.
Could you check if my reading value is correct or not?
P4_R72-R75 = 0x7FE648C6 (default : 0x7FFFFFFF) P4_R76-R79 = 0x8019B73A…
Part Number: PCM6020-Q1 Hi team,
Is there a risk under the normal operating condition to put the device into its test / diagnostic mode which should be used only for your(TI) debug or manufacturing purpose?
regards,
Part Number: PCM6020-Q1 Hi team,
Could you advise the typical and maximum supply current for Iavdd/Ibstvdd/Iiovdd under the condition below?
Mode : slave mode
fs = 384kHz
BCLK = 64 x fs
MICBIAS = 9V (AC-coupling) @Rext=4.7kohm
I2C bus
regards,
Part Number: PCM6020-Q1 Other Parts Discussed in Thread: PCM6240Q1EVM-PDK Hi Team,
Would you advise can TI provide EVM of PCM6020-Q1?
What's the EVM name for order?
Thanks
Best regards,
Shidara
Part Number: PCM6020-Q1 Hi team,
Regarding to PCM6020-Q1 power up/down sequence.
1. tf
Is there tf requirement?
2. What is the concern if tr is higher than 1 V/μs?
regards,
Part Number: PCM6020-Q1 Hi team,
SNR of 0dB single-ended mode for PCM6040 should be 110dB - 6dB = 104dB, correct?
If the input is 2Vrms, then SNR should be 104dB - 8dB = 96dB
Is my understanding correct?
regards,
Part Number: PCM6020-Q1 Hi team,
BSTOUT voltage is not specified in the datasheet, but only MICBIAS is specified.
Could you give me how much is the BSTOUT voltage?
WIll it change based on the MICBIAS setting to minimize dropout voltage at MICBIAS regulator…