Part Number: PCM6260-Q1 Tool/software: Hello TI support team,
How should I interpretate top marking in your device PCM6260QRTVRQ1 to know the DC? Example below.
Thanks,
Arturo.
Part Number: PCM6260-Q1 Tool/software: Hi expert,
I see from datasheet that we need config ADC channel gain before power-up.
How to understand power-up? We need config channel gain after enable micbias/en channel?
My customer is using external micbias…
Part Number: PCM6260-Q1 Tool/software: Hi expert:
We encountered a strange phenomenon in the CODEC circuit.
When AGC is ON, the recorded sound from the microphone has distortion(noticeably glitches), but this issue is resolved when AGC is OFF…
Part Number: PCM6260-Q1 Other Parts Discussed in Thread: SN74LXC2T45-Q1 Tool/software: The IO level of the used SOC is 1.2 V. The IO level of the PCM6260 is 3.3 V. The maximum bit rate=384(kHz)*32(bit)*4=49.152M
Please help recommend or evaluate:
①Please…
Part Number: PCM6260-Q1 Tool/software: We tested the TDM waveform quality of PCM6260 on PCBA PCM6260 has two requirements for TDM signals, td(SDOUT-BCLK) and td(SDOUT-FSYNC) Currently, the measured value exceeds the MAX value required by PCM6260 , which…
Part Number: PCM6260-Q1 Tool/software: Hi Team,
In PCM6260-Q1 datasheet that VBAT_IN pin is used for input voltage monitoring.
We're evaluating the current consumption of the entire system so we want to know the current consumption on this pin. …
Part Number: PCM6260-Q1 Tool/software: Hello team,
What's the difference between PCM6240 and PCM6260 about the function?
From the two datasheets ,pin 3,4,5 is different while other pins can be pin-to-pin.
About PCM6260,if the voltage of VBAT is 12…
Part Number: PCM6260-Q1 Tool/software: Hi expert,
How can we test the audio performance of PCM6260-Q1?
Can we use Audio precision to test it's SNR/THD/interchannel isolation?
Thanks!
Part Number: PCM6260-Q1
Tool/software:
hi expert,
my customer use PCM6260-Q1, they use two mic input, the two mic is the same, and first channel is differential mode, second channel is single end mode. the gain is the same for two channel.
The signal…