Part Number: PCM6260-Q1 Tool/software: Hi Expert,
My customer is using differential input microphone in automotive application, the cable is long but it's hard to find a GND pin from connector to connect shielding layer.
Do we need shielding twist…
Part Number: PCM6260-Q1 Hi TI,
We would like to know if there is a latest pcm6260 driver compatible with kernel 5.15 that can be provided to us? Thanks
Part Number: PCM6260-Q1 Other Parts Discussed in Thread: INA121 Hi
Customers encountered new problems when using pcm6260. Two of them were related to channel gain adjustment and automatic gain controller.
1. Situation 1: When I fix CH1_CFG2 Register…
Part Number: PCM6260-Q1 Tool/software: Hi expert,
My customer wants to use 6260 to measure an analog signal from DAB system. They plan to use line in mode for one channel.
What will change if I switch mircophone input to line input for channel config…
Part Number: PCM6260-Q1 Hi team,
One question would like to check with you. One of the input to PCM6260 is the AC differential signal(0~3.3V). Below is the schematic for PCM6260. You can find the AC input portion(SPK+, SPK-) in the red box.
I would…
Part Number: PCM6260-Q1 Other Parts Discussed in Thread: PUREPATHCONSOLE Hi
The customer's board currently has two PCM6260s installed. GPIO1 has been connected to a GPIO interrupt. But no matter how you adjust the register setting value of the bin file…
Part Number: PCM6260-Q1 Hello,
we are planning to use this PCM6260QRTVRQ1 IC for Audio ADC over I2s interface, pleases let us know where is the linux driver source available for this.
Part Number: PCM6260-Q1
Hello,
Our project is using PCM6260-Q1, and we both used GAIN and Volume parameters.
I want to confirm the amplification mode about this two parameters, but i didn't find any introduce from datasheet.
Can you help and tell…
Part Number: PCM6260-Q1 Hi
1. Could you help check the PCM6260 schematic , and any need to adjust
2 . The EVM line of pcm6260 has I2C and EEPROM on it. Could you please help me to confirm this function? Is it necessary to use it? Do you need specific…
Part Number: PCM6260-Q1 Hi team,
For PCM6260-Q1, for example, single-ended input amplitude is V=2V, differential input amplitude is V=1V, so actual input voltage=(V+) - (V-)=2V.
From our understanding, the ADC conversion results should be the same…