Part Number: PCM6360-Q1 Hi Team,
The maximum output current of MICBIAS in PCM6360-Q1 is only 80mA. Customer needs 120MA max Current.
Can customers use other power supplies as the bias voltage of MIC instead of using the MICBIAS voltage supply of PCM630…
Part Number: PCM6360-Q1 Hi,
do we have timing sequence for power up.
customer used to: power up 6360, then initialize 6360, then give MCLK, then BCLK, tehn get TDM
and they want to adjust it to: give MCLK, then power up, then initialize....
is there…
Part Number: PCM6360-Q1 Hi Team,
DATASHEET wrote above, HVDD needs to be greater than MICBIAS.
Some question as below:
1. If both HVDD and VBAT are 8V, and MICBIAS is also configured at 8V, what will happen?
2. If both HVDD and VBAT are 8V, and MICBIAS…
Part Number: PCM6360-Q1 HI,
We'd like to pick your brain about the similar PCM6360 discontinuous waveform question.
We input a continuous waveform (CH1) and get the output which is dicontinuous. The signal train is ADC-DSP-DAC, which in counterpart…
Part Number: PCM6360-Q1 Other Parts Discussed in Thread: PCM1865
Hi,
Here we have a project designed in with PCM6360Q1 which has built in PGA besides digital volume control. We need a sensitivity range from 7V to 200mV with this project. But when we apply…
Part Number: PCM6360-Q1
Hi team,
Our customer have a question about the PCM6360-Q1.
The Input Line in is the 1kHz signal source, and the output is output disconnected.
As the pictures shown, the yellow is output and the green is input.
The content of the…