Part Number: PCM9211 Hi,
Currently, I'm using PCMDEVICE codec driver for PCM9211. But, I found the function: pcmdevice_regmap_read() always returned error meaning reading pcm9211 registers failed. I debugged the code, but didn't find the solution.…
Part Number: PCM9211EVM-U My NEW PCM9211EVM just arrived, but I face same issue as Mr Zhamilya Zhamilya (18 days back), i tried on two laptops (win 11) , The code control software fails to connect , it says "Communication error", but the EVM is detected…
Part Number: PCM9211 Hi team,
I would like to ask a few questions.
Question 1 Please tell me if the following operations are possible at the same time.
AES/EBU and SPDIF signals input to A are output to B in I2S format. Reclock the AES/EBU and SPDIF signals…
Part Number: PCM9211 Hi expert
Would you please help to ensure if DIX9211PTR and PCM9211 belongs to the same family?
Which is the difference between them.
Part Number: PCM9211 Hi, TI support team
A partial circuit review request has been received from the customer.
Reference caps connected to pins 44 and 46. The value is 10uF and is written in the datasheet, but to improve the sound quality, we are going…
Part Number: DIX9211 Other Parts Discussed in Thread: PCM9211 , Hello,
The question is in tite: difference between DIX9211 and PCM9211 ?
Thanks.
Sincerely,
Pavel.
Part Number: PCM9211 Hi team,
I have a same question as this thread: https://e2e.ti.com/support/audio-group/audio/f/audio-forum/650937/pcm9211-automatically-mute-the-dir-in-case-non-pcm?tisearch=e2e-sitesearch&keymatch=non-pcm#
This thread hasn't…
Part Number: PCM9211 Hi,
Customer inputs the I2S signal from an external device into the PCM 9211. And the customer wants to input the I2S into the DIT and do the SPDIF conversion. Could you answer the following questions?
1. Could you tell me the timing…