Part Number: PGA2311 Other Parts Discussed in Thread: PGA2310 Hello,
I am operating PGA2311 under +/-5V analog supply. Since it is presently unavailable in stock for the quantities I need, can I buy PGA2310 in its place? SOIC version. Will work it work…
Hi Timothy
how was the holidays? hope all went well :)
well, i was not sure that the board i design to the PGA2310 was ok so to eliminate this suspect i ordered the PGA2310 EVM.
now i must say, it is final, the PGA clicks in every way, even in the EVM…
Hi Ian,
Thanks for the information.
I just brought ICL7660, it also works as voltage inverter. but I have another problem.
I have connected the PGA2311 by the typical application in figure 13 from the datasheet ( www.ti.com/.../sbos218d.pdf)
While streaming…
Other Parts Discussed in Thread: PGA2310 If an audio signal arrives to the pre-amp/vol control from a class A source, one would want to keep it that way all the way to the class A power amp. In the case of a passive (purely resistive) volume control, …
Other Parts Discussed in Thread: PGA4311 , PGA2310 Dear All,
Let me ask the specification of these products. ・PGA4311 ・PGA2310 Please tell us Slew Rate [V/μS] of these products.
Best Regards, Tsuguhiko Asai
Other Parts Discussed in Thread: PGA2310 , TAS5414C , TAS5414C-Q1 , TPA3111D1-Q1 We are looking at PGA2310 to use is as audio amplifier.
We need about 5W output.
Also It needs automotive q-100 qualified.
Can you check that I can use it as a audio amp.
Or If…
Hello,
I think Frank was right. I ordered a PGA2311 as a sample and replaced my PGA2310 with it, and noise almost has gone!
I think it is because of the 9.5uV output noise of PGA2310. PGA2311 has 2.5uV noise and it seems low enough to hear almost no noise…
Other Parts Discussed in Thread: PGA2310 Hi,
i have started making a hi-fi stereo preamplifier. The preamp has a very quiet background until I connect my graphiq eq into the signal path. When the eq is connected into the signal path I can hear a high frequency…
Other Parts Discussed in Thread: NE5532 , PGA2310 , PGA2310EVM Hi all,
I have the pga2310 between the DC decoupled buffer and DC coupled summing amplifier. Both the buffer and the amplifier are NE5532. At power on I hear a loud click and the oscilloscope…