Part Number: PGA280 Other Parts Discussed in Thread: PGA281 ,
Good day,
In a lot of the reference designs that utilize the PGA280/281 (Including the SBOM817 TINA File for PGA281), I see some light load resistors added to the PGA Output (2.5K in the case…
Part Number: PGA280 Other Parts Discussed in Thread: OPA192 Hello TI,
Is there any data or specifications for the off-state leakage current of the input switches (A1/A2 & B1/B2)?
I would like to connect them to very high impedance inputs in order…
Part Number: PGA280 Other Parts Discussed in Thread: PGA281
Hello,
With regard to the VOCM pin, the datasheet always shows this connected to mid supply (VOP+VON)/2
Is there any harm to performance in setting VOCM off from center? I don't see anything…
Part Number: PGA280 Hi teams,
Can you help me about the questions?
Will error flag OUTerr be triggered only by overcurrent?(see the pic below)
If so, what’s threshold?
Part Number: PGA280 Other Parts Discussed in Thread: PGA870 Hi,
I am new to analog circuit design and I need to design the analog front end for a CCD imaging system (Pushbroom camera). I am using the TCD2905 RGB linear CCD and the LTC2246 ADC. I need…
Part Number: PGA280 Other Parts Discussed in Thread: TL7660 Hello:
I wanted to check if I can bring in single ended analog signals into the INxa inputs of the PGA280, or do I need to bring in a differential pair to take full advantage?
If I can bring in…
Part Number: PGA280 When debugging the PGA280, we sent the hex instruction 8300 to the PGA280 register 3 "set BUF time-out" (as shown in the figure). It should have got a return value of 19, but we did not receive any value, and the PGA280 did not respond…
Part Number: THS4551 Other Parts Discussed in Thread: PGA281 , PGA280 Hello,
I wonder if it is feasible to use THS4551 Vocm pin as an output to feed the PGA281 Vocm input. Supposing Vocm would be Vcc/2
I understand from previous discussion here at forum…
Part Number: PGA280 Other Parts Discussed in Thread: PGA281 , PGA103 , PGA202 , OPA2320 Hi team,
Our customer uses PGA280 + AD7765 for signal acquisition
Short the input of AD7765, the noise level is low. However, when PGA280 + AD7765 are tested together…