Part Number: PGA300 Hello,
I calibrate PGA300 with EVM and GUI.
I have a problem with calibration, so I would like some advice.
Until a while ago, I was able to calibrate without problems.
When I was conducting an accuracy verification test after…
Part Number: PGA300PGA300, 4 to 20 mA mode, DAC Code Calibration:
When read and write DAC code
1) when 4 mA, reading was always very close to 4 mA
2) when 12 mA, reading was always very close to 12 mA
3) when 20 mA, sometime reading in amp meter was…
Part Number: PGA300 Hello,
I don't know how calculate AD value of PGA300 EEPROM from PGA300 GUI voltage value. I would like to write AD value to PGA300 EEPROM by OWI communication that I prepared instead of GUI. The following are the items I want to attempt…
Hello Hironari,
The reason why devices such as the DRV421 are not paired with the PGA300 is that these are very different devices.
The DRV421 is a fluxgate current sensor and the PGA300 is a Signal Conditioner and Transmitter for Pressure Sensors.
Here…
Hello! We appreciate your interest in this device, however at this time we are unable to offer additional support. Please use our extensive resources – including datasheets, user’s guides, application notes, FAQs, and existing E2E posts – to guide your…
Part Number: PGA300 Hello,
I would like to know following requirements of OWI communication.
1) Cable length
2) Cable thickness
3) Baud rate
4) Loop resistance (Termination resistance)
I think Baud rate is decided after recomendation cable length, type …
Hello,
Yes, I compared results between GUI and DLL about 4P4T and 3P3T. In that time, 4P4T results were absolutely muched between GUI and DLL, but 3P3T results were not same between GUI and DLL.
In 4P4T, if GUI results were success, DLL output coefficients are comple…