Part Number: PGA305 Hello TI Support Team,
We are using the PGA305 IC in a pressure-sensor. Our test sensor specification is:
Range: 0–1000 bar
Output: 4 mA at 0 bar, 12mA at 500 bar and 20mA at 1000 bar
Calibration points: 0 bar at…
Part Number: PGA305 Tool/software: Hello,
Best wishes for 2025.
I have a question regarding the PGA305.
Given that the operating temperature range is [-40,150]°C, I would like to know that if the PGA is well thermally insulated (that it always remains…
Part Number: PGA305 Tool/software: hi,
is it possible to have a complete datasheet of the PGA305 component? Available datasheet on TI web site seems to provide only general information.
We would like to know, current consumption, start time,.... …
Part Number: PGA305 On PGA305 EVM when using GUI (PGA305 EVM)
I have a problem with "Accuracy Verification Test"
After successfully completing the "Guided Calibration" and getting the correct results on the voltage output.
At the beginning of…
Part Number: PGA305 Tool/software: Hello,
this happened with 3 PGA 305's : First, i can read an write into the EEPROM but at some point (when a another write operation occurs) i cannot read or write inside the EEPROM. I can still set the 0x0C register…
Part Number: PGA305 Tool/software: Hi,
We are currently having some issues with OWI activation that seems to be related to DAC in 4-20mA mode.
After OWI activation when we are trying write to DAC we found that we can not write directly the DAC value…
Part Number: PGA305 Other Parts Discussed in Thread: PGA900 Tool/software: We are currently producing a product that incorporates the PGA305. This product outputs a 4–20 mA current signal in response to pressure detected by a sensor.
However, for the…
Part Number: PGA305 Tool/software:
Hello, I am currently a developer working on connecting an external load cell to the PGA305. After reading the PADC values, I plan to use a calibration process to convert them into kilograms…
Part Number: PGA305 Hello everybody,
I have a question regarding configuring an external PGA 305 to the PGAXX EVM using OWI cominucation.
I can read data from my PGA305 when the PGA305 is in the PGAXXxEVM. I would like to do the same on a PGA305 already…