Part Number: PGA411-Q1 Tool/software: Code Composer Studio Hello?
I reviewed application report, I saw "pga411.c and pga411.h" in "Software Developer’s Guide for PGA411-Q1(July 2016)".
But I can't find these files.
Now, isn't these files published…
Part Number: PGA411-Q1 Hello,
We have designed our custom board using PGA411-Q1 IC, but we are not able to read the registers through SPI. The booster circuit is not working, and is only providing 5V where 12V is expected.
Can someone help in resolving…
Part Number: PGA411-Q1 Hi,
I am trying to use the PGA411-Q1 EVM with a resolver that has 4 terminals. The terminals on the resolver are "Power Ground", "Resolver Sine", "Resolver Cosine", "Resolver Drive". I assume that I can connect the negative side…
Part Number: PGA411-Q1 Hi Team,
May I ask about the potential influence of PGA411-Q1 external crystal accuracy? Is 100ppm(whole temperature range sufficient enough)?
Thanks.
Best Regards,
Livia
Part Number: PGA411-Q1 I do it according to this circuit. The pga411 doesn't work. I don't know if there is a mistake in the circuit diagram. Rotary encoder v1.0.Sch
Part Number: PGA411-Q1 Hello, expert, I would like to inquire about the technical issues related to PGA411-Q1 ,when decoding the motor speed, the decoding speed is always unstable, and there are irregular fluctuations, and the fluctuation is obvious.…
Part Number: PGA411-Q1 I have designed a resolver to digital converter board using PGA411-q1 IC. I have taken the help of the PGA411-EVM and the main datasheet, but there are many things involved in it. Like the EVM has got its own DSP and GUI, but I…
Part Number: PGA411-Q1 Hello, everyone!
I'm using a resolver to digital converter, PGA411-Q1, to get angle information of the motor rotator. I have set PGA411-Q1's pin the following.
OMODE: High BMODE0: High VA0: LOW VA1: HIGH
However, no ORD[11…
Ashkan,
The PGA411-Q1 has internal temperature diagnostics, so the device cannot be used above the rated temperature. By 200 degrees C, thermal shutdown will occur.