Part Number: PGA450Q1EVM Other Parts Discussed in Thread: PGA450-Q1 , PGA460 , PGA460-Q1 , TPS4H000-Q1 Hello TI -Team ,
i ma working on Automotive ADAS application project for reverse park assist , we are using 4 ultrasonic sensors , i have gone through the…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: TIDA-00151 , PGA460 Hi TI support Team
This is for an parking assistance application (automotive).
We are planning to use the PGA450 based driver along with the Ultrasonic Transducer MA58MF14-7N from…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: USB2ANY , PGA450Q1EVM , Hi,
Apart from TI-GER board, please confirm if the USB2ANY adaptor can be used to interface between the PGA450Q1EVM GUI (in PC) to the PGA450Q1EVM-S.
Or, any other standard…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA460-Q1 , h ello everyone ,
i am looking for automotive ultrasonic sensor with LIN protocol compatible with hercules ( TMS570lS1224 ).
detection range ( 10cm up to 3m).
is there any recommandations …
Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA450Q1EVM Are there any recommendations for OSC_SYNC_CTRL vs CLK_SEL setup scenario? I've experienced some issues when OSC_SYNC_CTRL had other than programmed value - I noted the difference between…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA460-Q1 , PGA460 , MSP-EXP430F5529LP , BOOSTXL-PGA460 Software development guide for PGA450 mentions using Keil C51 Development Tool for 8051 devices. Can we use other 8051 development systems like…
Part Number: PGA450-Q1 Hi,
Is there any other suggestions / recommendations for an off-the-shelf mass production tool, besides Acroview AP8000 for mass programming?
Thanks,
Eyal
Hi Jakub,
The PGA450-Q1 does not include the same system diagnostic features as the PGA460-Q1. We are aware that the PGA450-Q1 suffers from a long dead zone, where you can only reliably detect downwards of about 30cm. The PGA450-Q1 only includes a decay…
Hi Bart,
To properly debug this, it is best to readout the entire ESFR register space of the both the DEVRAM device and the OTP device for comparison. There is no reason the OTP and DEVRAM modes should behave differently in receiver sensitivity when the…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: TIDA-00151 , PGA450Q1EVM , , TUSS4470 , PGA460 , PGA460PSM-EVM Hello,
we are integrating a PGA450-Q1 on a custom board programmed with example program: PGA450-Q1_TIDA-00151_OTP-UART.hex. We are trying…