Part Number: PGA460-Q1 Other Parts Discussed in Thread: PGA460 , , BOOSTXL-PGA460 Hello Ti team,
I am working with the PGA460 on a custom PCB that includes an ultrasonic transducer and an external controller. Ultrasonic sensor is driven using the transfromer…
Part Number: PGA460 In my original post, I was looking for a way to detect the source/direction of ultrasonic noise at a specific frequency using the PGA460 board. This was needed because we have multiple valves and industrial equipment near an ultrasonic…
Part Number: PGA460 Question 1: Does the PGA460 support a 100 kHz ultrasonic transducer? Question 2: The operating frequency of the transducer on the evaluation board is 58 kHz, and the operating frequency of transformer T1 (TDK B78416A2232A003)in the…
Part Number: PGA460 I am experiencing an issue with the PGA460: During rapid and repeated power cycling, the device may work abnormally with some probability. The only way to recover is by restarting the PGA460. However, since the mainboard lacks a hardware…
Part Number: PGA460 Hello TI Team,
I am currently working with the PGA460 ultrasonic signal processor using a 40 kHz ultrasonic transducer on a custom PCB. I have configured the device by writing the following parameters into EEPROM:
/* USER_DATA1…
Part Number: BOOSTXL-PGA460 Other Parts Discussed in Thread: PGA460 I have just started using BOOSTXL-PGA460 for development. I followed the user manual and used the LP-USB power mode, along with the muRata MA58MF14-7N transducer for short-distance measurement…
Part Number: BOOSTXL-PGA460 Other Parts Discussed in Thread: MSP-EXP430F5529LP , PGA460-Q1 Hi Expert,
Does the BOOSTXL-PGA460 bundle include the MSP-EXP430F5529LP LaunchPad , or does it need to be purchased separately?
Thanks
Daniel
Part Number: BOOSTXL-PGA460 Other Parts Discussed in Thread: PGA460-Q1 I am using the BOOSTXL-PGA460 for a capstone project. I have measured the power consumption of the whole board but was wondering if I could measure the power consumption of just the…
Part Number: PGA460-Q1 Tool/software: Hello Forum,
I want to know if there is a possibility to average the DATA DUMP over 5 measurements?
wobbling Data Dumps are not very helpfull.
Many Thanks in advance for your answers.
BR's
Martin
Part Number: PGA460-Q1 Other Parts Discussed in Thread: PGA460 , EVM430-FR6043 , MSP430FR6043 Hi,
I intend to build an anemometer using 3x PGA460 to determine the wind speed and direction. They will be connected on the same UART port of the MCU and…