Hi, I come back here after a while, because I finally found what was causing my issues. Long story short : I managed to get a few PGA900 in VQFN format, and after a bit more of testing I got why I was always programming on the OTP. When I started programming…
Part Number: PGA900 Hi:
We meet a strange issue that PGA900 output will be 4.85V( intenal fault output signa) when board power on and keep be 4.85V for about 3 to 4 seconds then back to normal output 0.5V.
The AFEDIAG shou 0x66( We don't use TGAIN) when…
Part Number: PGA900 Customer has PGA900 questions related to baud rate:
For an embedded application, we are trying to run the UART as fast as possible. We have found that setting BAUD_RATE to 0x0002 and larger (I.E 83.333KB and slower) seems to work…
Part Number: PGA900 Other Parts Discussed in Thread: TLIN2029A-Q1 Hi,
I just found the PGA900 while desperately looking for a replacement of a SSC-IC with integrated LIN interface. I was asking myself whether it is possible to connect the PGA900 through…
Hi Tomy,
Oh I understand the problem now, I apologize.
The GATE pin's purpose is to regulate the voltage down around 3.5V, you have to disabled the regulation feature (and put the MOSFET into the saturation region) when you want to communicate with…
Part Number: PGA900 Hello,
I have a question regarding the programming of the PGA900, and I couldn't find a straight answer in the questions already asked on the forum. Is it possible to use the XDS110 probe to program the PGA900, instead of the XDS200…
Part Number: PGA900 Hello, I installed PGA900 GUI software along with labview runtime 2012 on my PC (Windows 10 Pro, 21H2). When I tried to launch the PGA900 GUI sotware, it showed the below error message.
Sorry, it is Japanese, but it says
Labview runtime…
Kim,
Scott is on travel, so I will help while he is out. When you mention " some PGA900 is a voltage near ground ", are you saying that you have built multiple modules and some of these modules behave correctly and others will output a bad voltage near…
Part Number: PGA900 Other Parts Discussed in Thread: UNIFLASH ,
Today ,I used the XDS200 to download the firmware to the PGA900. but sometimes the uniflash showed it's failed, but I check the target memory , it just downloaded some code into it .
…