Part Number: PGA970 Hi Team,
We are trying to generate Vrms for Primary winding of LVDT. P1 and P2 are directly link to P1A and P2A through jumper settings. The configuration screenshot of GUI as below:
Through this we are able to get 1.25Volts Peak…
Part Number: PGA970 Hi Team,
We are trying to get AC excitation for LVDT . On primary P1A we are getting sine wave in PGA970GUI waveform generator. On TP71(P2A) the Sine wave is not appearing . Could you please help me to find a solution for getting Sine…
Part Number: PGA970 Hi,
I have procured PGA970 EVM Board along with USBTOANY. I want to connect and give excitation to LVDT. LVDT is MHR 005 from TE Connectivity. Below are the details of LVDT:
and planning to excite at 2.5kHz & electrical specification…
Part Number: PGA970 Hi! Odd question here. Our application of PGA970 has multiple PGA970 that read data from 6-wire RVDT's.
If the Excitation (primary windings, P1/P2) of a single PGA970 is wired to a RVDT/LVDT, and then the secondary windings(S1P/S1N…
Part Number: PGA970 Other Parts Discussed in Thread: USB2ANY Hello,
I programmed the PGA970EVM with XDS200 with "pga970_Generic_1.6", but I always get this message:
Error connecting to the target: (Error -1266 @ 0x0) Device is held in reset. Take…
Part Number: PGA970 Hello,
I have to use external voltage reference for primary-side excitation. Also, I have two wires interface from RVDT (two windings connected in reverse internally of sensor).
Is it possible to use S1 input as reference voltage input…
Hi Tam Vu,
There is a request link for the full data sheet on the product landing page for the PGA970 . Part way down on the web page page you will see a link inside the More Information block. Click on the Request now link.
Best regards,
Bob B
Hi Bob,
after I test SPI signal Both side of U7 (MOSI, MISO, CLk, CS) I realized that PGA970 worked but not completely, I measured all voltage and TPs again I got that maybe Half of the PGA970 works, I mean sensor side was broken, I decided to remove…