Part Number: UCC28700-Q1 Other Parts Discussed in Thread: UCC28700 , PMP10200 , UCC27517A , UCC28730 Hello,
I want to use the PMP10200 reference design, but the UCC28700 controller used in this design is quite old.
Can you recommend a newer generation…
Part Number: PMP10200 Other Parts Discussed in Thread: UCC28700 , Tool/software: Hello-
I'm looking to develop a high power (10's kW) DC/DC converter to drive a heater load. PMP10200 outlines an application of the UCC28700 for at least the core of a…
Part Number: PMP10200 Other Parts Discussed in Thread: UCC28700 , We have isolated DC-DC power supply requirement as per below data.
Input voltage range 24DC to 500VDC 50Hz & 60Hz
Output voltage +15VDC @ 1.3A, -15VDC @ 200mA
Output wattage requirement…
Part Number: PMP10200 Other Parts Discussed in Thread: UCC28700 , I'm trying to figure out why the output power is specified as 20W when input is higher than 60V, but only 10W otherwise. Based on my quick math, it seems like the converter should be able…
Hi
As I previously shared, PMP10200 is an example design with that demonstrates support for output voltage from 25VDC and 520VDC, which is 20.8x. This reference design is highlighted in the related documentation section of the app note you referenced…
Hello,
The UCC28700 should have similar protection functions compared to the UCC28636. The input under voltage is easier to setup. The device has OCP, OVP and input UVLO shutdown.
I found this UCC28700 reference design that has an input of 25VDC…
Hi Stefan,
Thank you for the reply.
Before trying to answer your questions, I would recommed a couple of designs which might be in the voltage range you are looking at since trying to get UCC28631 work might be difficult.
PMP10200: https://www.ti…
Hello,
I found a reference design using the UCC28700 for a 25V to 500V input range with 28V output. This is a 10 W design. This could be used up to a 60 W design by changing the transformer.
The UCC28630 uses a similar control law and it may be…
Part Number: UCC28700 Other Parts Discussed in Thread: PMP10200 Hi Team,
I need a controller recommendation for a full-bridge isolated boost topology, similar to what is shown below.
The current specs I have are the following...
Input voltage…