Part Number: PMP10506 Hi E2E,
The input voltage of PMP10506 is 9V to 60V, but voltage rating of C12 is only 25V in schimatic.
Can it be understood that when the input voltage increases, the Vin pin can maintain a voltage below 25V?
Thanks!
Hi, Kevin,
Q1; It should be ok to put output capacitor with 4*22uF,6*100uF and 1*680uF EC.
Q2: Now, since convert could output full load. There is only improving dynamic response. I would suggest to fine tune decreasing C15 firstly , and adjust R23, C14…
Part Number: PMP10506 Other Parts Discussed in Thread: PMP Hi, E2E
I refer to PMP 10506 to make a circuit board.
But some issues need to be fixed.
Issue 1: I measure the Vout as 5.2 to 5.1VDC, depending on the Iout value. I want to adjust the Vout to 5.0VDC…
Hello Larry, Thanks for reaching out to us via e2e.
There are three reference designs on our website which are utilizing the LM5122 for an isolated or non-isolated flyback design:
www.ti.com/.../PMP7992 www.ti.com/.../PMP9256 www.ti.com/.../PMP10506
You…
Part Number: PTB78560A Other Parts Discussed in Thread: LM5122 , LMV431A , PMP10506 The device PTB78560AAH is showing a NRND warning in the website listing and on vendor sites. Is there a device that is equal to this device that would be recommended for…
Thank you very much for responding in constructive way. Now I am considering PMP10506 for our design due to
1> we are developing Industrial PC,linux arm cortex A7 , 700 mhz. Here next version will be for quad cpu on linux platform.
2> next version…
Other Parts Discussed in Thread: LM5022 , LM5160 , LM5015 , LM34927 , TPS2660 , LM5022-Q1 , PMP10506 , LM5122 , LMV431A , TPS2511 , TPS54340 , PMP9253 , LMV431 , TPS40170 , TPS54340-Q1 , TPS2400 Hello, I have read many posts in order to find a solution that best fits…
Bell,
Since this is a very unique spec target, it's hard to find an existing TI Design that's a close match.
You can search the available TI Designs and reference designs here:
www.ti.com/.../refdesignsearchresults.tsp
If you click on the tab…
Sneha
If you search TI DEsigns by parameters, you get an interactive page where you can specify your input voltage range, output voltage, output current, AC or AC inputs, isolated or non-isolated, etc. The tool will gradually narrow the number of matches…