Hi Jerome,
I made a mistake and looked up the wrong design (PMP10532).
You are right the input range is 10-14V, in order to change to 24V input and keep the same transformer, you would have to make a lot of other changes.
Probably changing the primary…
Hello,
One option would be to the LM5160A which is a flybuck device. You can find the product folder at this link: www.ti.com/.../LM5160A You can find a reference design at this link: www.ti.com/.../PMP10532
A second option would be to use the LMR36015…
Other Parts Discussed in Thread: LM5160A , PMP10532 , LM5160 Hi All,
is it possible replace LM5160 on same circuit with LM5160A. Are there some difference between two component ? The reference project is PMP10532 but it works with WSON package.
…
Hi Bernard and Bhavdipsinh,
Thanks a lot for prompt help, since there are multi outputs, we may propose the below solution,
We have PMP10532 based on LM5160 cover the following
+12V 0.25A
±5V, 0.3A (isolated)
And PMP9253 based on LM5022 cover…
Part Number: TPS54335A Other Parts Discussed in Thread: LM5160A , , TPS54308 Hi, team.
My customers are looking for devices under the following specifications,
I have proposed at LM5160A and TI-design ( www.tij.co.jp/.../PMP10532
<Specification…
Other Parts Discussed in Thread: PMP10532 Hello Sir,
I am designing a power rail where I have multiple power rails.
1V, 1.2V, 1.8V, 3.3V etc.
plus I have operational amplifiers on my board for which I need a dual supply (+-12V, +-7.5V).
I want…
Hello,
We are nearly through the release of a new Circuit document that describes this use case. Please find the nearly published version attached. The final version should be online in the next couple of weeks but the main information won't change…