Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: PMP11155 , UCC28063A , PMP10116 , UCC28050 hi
I have a project for HV ceiling fan, so I want a solution spec is
Vin: 82VAC~220VAC
Vout: 310VDC
Iout:2A~3A
does TI have any reference design can provide
Vineet
UCC28056 cannot meet your PF requirement when configured as a flyback. If you would like a PFC flyback our 8 pin PFC controller UCC28050 can meet your PF requirements. PMP11155 is an example of it working as a PFC flyback close to your target specifications…
Hey Amol,
I'm glad that your snubber is not burning anymore!
The calculator tools are definitely helpful, and are there to help start designs and guide users along the way on component value selection. They are not a way to guarantee operation of…
I think you might be better off with a single stage PFC flyback converter.
The following link will you to an 85V to 265V AC in to 24V 1A reference design using the UCC28051. The transformer turns ratio should be correct for your design. However you will…