Hi Navi,
Sorry for the delayed response. Please see my answers to your questions below:
1. While not designed for 75VAC to 275VAC, this design will still operate across that range.
2. The output voltage can be adjusted by changing the value of R16. A…
Part Number: UCC28710 Hi,
We have a design based on PMP11185 using the UCC28710. It is targeted for 5V / 2A output to power a small BLDC inverter. Our power supply design is almost identical to PMP11185, including the Wurth transformer.
We notice that…
can i replace the RLTI-1061 Tx and replace it with 750315526 Tx (435uH) as used in
85-265VAC Input, 5V/2A PSR Flyback Reference Design
(ACTIVE) PMP11185
www.ti.com/.../tidrhg1.pdf
and still get the same result?
Dan,
For an outdoor industrial application, if reliability is the key care-about, then in reality the environmental stresses (temperature, humidity, shock/vibe, immunity to electrical surges/transients/external interference) and the PSU mechanical design…