Part Number: UCC28061-Q1 Other Parts Discussed in Thread: UCC28070-Q1 , UCC2818A-Q1 , UCC28063 , UCC28061 , PMP11282 , UCC28060 , UCC28180 , UCC2818 , UCC2818A Tool/software: Hi TI Team,
Can you suggest an automotive analog PFC controller for the following…
Hi,
There is an updated design built on PMP11064 PCB:
www.ti.com/.../PMP11282
The output voltage was adjusted to 24V for better efficiency.
This design is designed without forced air cooling (natural convention). So you don't need to provide additional…
Ted
Our PFC boost controllers can be configured to work as a flyback. Below are some reference design examples
1 phase TM
http://www.ti.com/tool/PMP9730
Interleaved TM
http://www.ti.com/tool/PMP10116
http://www.ti.com/tool/PMP11282
…
Hi Murthy,
sorry that TI don't have new full bridge LLC , but you can refer the reference design as below link, which meet your spec.
https://www.ti.com/tool/PMP11282
Hello Adam,
Thanks for posting this question.
Do you need 20A continuously/nominally or is that a peak requirement? (This will help clarify which topology is best suited for your power level)
If you're planning to use analog control, the following…
Dear Sir,
Please find attached the captured waveform showing 5–6 cycles of the line voltage and the scaled-up line current.
I have used the same reference design PMP11064 for testing. The current test conditions are Vout = 20 VDC and Iout = 1…
Part Number: UCC27524A Tool/software: Dear TI Team,
Please find attached the reference circuit I am using. I am implementing the UCC27524AD as a driver in an interleaved PFC boost circuit (as per the attachment).
Currently, I am observing proper PWM…