Part Number: PMP22419 Other Parts Discussed in Thread: UCC28740 , UCG28826 , UCC28056 , BQ24600 Tool/software: Hi Team,
I am working on a Li-Ion battery charger. Below are the specifications.
Vin - 90 to 265Vac
Vout - 18Vdc
Pout - 100W
Cell…
Part Number: PMP22419 Other Parts Discussed in Thread: TIGER Tool/software: Hi team,
Please send me the file of PCB layout. In the reference design page, we only have the PDF file. Please help to check.
PMP22419 PCB (ti.com)
leo.yang@ti.com
Thanks…
Part Number: BQ25710 Other Parts Discussed in Thread: PMP22419 , CSD87355Q5D Using the reference materials for the PMP22419 board from the official website, I hand-soldered a motherboard myself and used the BQ25710, following the reference materials exactly…
Part Number: BQ25713 Other Parts Discussed in Thread: TIGER , PMP22419 Tool/software: Hello,
I am designing charger for my 3S2P Li-ion battery using BQ25713 charging IC, where the max charging current I will set will be 6A. I want to develop fast charging…
Part Number: BQ25720 Other Parts Discussed in Thread: TIGER Tool/software: Hi, I have based my design on https://www.ti.com/tool/PMP22419 .
This uses a 1.5uH inductor, my calculations suggest a larger inductance is needed.
In my design, the Vin…
Part Number: BQ25720 Other Parts Discussed in Thread: BQ25710 , , TIGER Hi Team,
What is the input current limit for BQ25710 and BQ25720.Which means what is the maximum current supported from 19V AC/DC adapter. From BQ25720 reference notebook design…
Part Number: BQ25730 Other Parts Discussed in Thread: PMP22419 , TIGER , BQ25750 , Hello,
We are working on development of Medical device.
Fundamentally, we would like to use the Ti part BQ25730 for our application which is described below.
Please…
Hi Humza,
We have a detailed schematic checklist for your reference. See below.
[FAQ] BQ25720: schematic checklist
I don't think you can process 240W with BQ25720. Assuming 95.4% ( PMP22419-140W design ), there is 11.6W power losses.
Two alternative…
Part Number: BQ25710EVM-017 Other Parts Discussed in Thread: BQ25720 , PMP22419 , BQ25710 , TIGER Hello,
Kindly share the altium schematics of the reference design used in BQ25710EVM-017
Thanks,
Khalid
Part Number: BQ25720EVM Other Parts Discussed in Thread: BQ25720 , PMP22419 , BQ25731EVM , BQ25723EVM , BQ25730EVM To speed up the design, I would like to get the Altium design files.