Part Number: PMP22477 Other Parts Discussed in Thread: TPS23730 Hi -
Can you help with these questions for customer application? They are using TPS23730 and referencing PMP22477.
T
In the spirit of trying to keep the design as small as possible…
Part Number: PMP22477 Other Parts Discussed in Thread: TPS23730
Tool/software:
Hi TI Team,
I can see in feature "Primary Side Regulation(No Optocoupler)", but in given schematic secondary side regulation is also there in www.ti.com/.../tidma48a…
Part Number: PMP22477 Tool/software: Hi team,
My customer wants to follow the ref design for a type 3, class 5 (40W) project, but the board space is limited.
1. Engineers are wondering which components of the below circuit can be removed.
2. Could…
Part Number: PMP22477 Tool/software: Hey,
While trying to implement the reference schematic, I ran into severe issues sourcing any of the T2 alternatives.
These are the ones listed in the datasheet:
LinkCom LDT9055-51R
Würth Elektronik 750320319…
Part Number: PMP22477 Tool/software: Hello team,
I am implemementing POE functionality on a board. We are basing the design off of PMP22477and want to know the reasoning behind using FETs/ FET-diodes over diodes in a 50W application. Is it due to efficiency…
Part Number: PMP22477 Tool/software: Hi team,
For the reference design of PMP22477, I see the hardware design with amplifiers, NMOS to get TYPE1, TYPE2 as below capture circled. Could you explain what is the function for this circuit? It seems that…
Part Number: PMP22477 Other Parts Discussed in Thread: TPS23730 , TPS23731EVM-095 , TPS23731 Hi team
I have design question of PMP22477.
If the power limit is type 3, may I reduce this circuit? as shown below
I think it about current sense (CS)…
Part Number: PMP22477 Other Parts Discussed in Thread: TPS23730 Dear All,
has the PMP22477 ben tested with FDMQ8205A active bridge?
Can you share the results of efficiency with FDMQ8205A regarding to the diode bridge solution?
Also can the…
Part Number: TPS23730 Other Parts Discussed in Thread: PMP22477 Tool/software: Hi Team,
I have a project that used TPS23730 with 12Vout/51W design, would it be possible to provide the actual PCB layout file in an Altium Designer .PcbDoc file format…
Part Number: TPS51113 Other Parts Discussed in Thread: PMP22477 Tool/software: Hi Team,
Design a DC-DC converter
Vin 20V, Vout 12V, Iout 4.16A 50W
This design requires current sharing and power limit functions.
When the current exceeds 4.16 A…