Part Number: PMP22650 Other Parts Discussed in Thread: TMDSCNCD280039C Hallo, I'm trying to debug a PMP22650 custom firmware with the controlCARD installed on the PMP22650 and connected via USB cable. I partially tested my firmware on TMDSCNCD280039C…
Part Number: PMP22650 Hi everyone,
I'm looking for two Cyntec magnetics from the PMP22650 OBC (On-Board Charger) reference design, which we are currently replicating:
Common mode choke: VI-20174A (Cyntec)
Transformer: VT-20163 (Cyntec)
These…
Part Number: PMP22650 Tool/software: Dear TI,
Can the below mentioned evaluation unit be purchased form TI or that is available for self build only?
TIDM-02013 AND PMP22650
Thank you for your feedback.
Have a great Day.
Zoltan
Part Number: PMP22650 Tool/software: I was exploring the control loop of CLLLC, and I have a few queries. Please help me with clarification.
1. On the secondary side of CLLLC, there is one block named Simple SR-Driver connected between the drain and…
Part Number: PMP22650 Other Parts Discussed in Thread: TMDSCNCD280039C , We are using the TMDSCNCD280039C control card. When we directly inject a 50 Hz AC signal with a 1.65 V DC bias into the TTPLPFC_VAC pin, all six PFC drive signals are output normally…
Part Number: PMP22650 Tool/software: I am trying to design the converter PMP22650 which has 2 daughter boards 22712 and 22773. The gerber data given in the design files is incomplete and is not having the inner 2 layers. I would like to have the complete…
Part Number: PMP22650 Other Parts Discussed in Thread: TIDM-02013 , , C2000WARE Tool/software: Hello Application Team:
My customer is plan starting develop 6.6kW OBC , we checked there have E2E thread update the ref design Final SDK in Q1 or Q2 of CY2022…
Part Number: PMP22650 Hello,
We have requirement of 48V Input ,4KW Output Isolated DC-DC Converter.
Input : 36V DC to 60V DC , 48V DC Nominal
Isolated Output power : 4KW
Output voltage : Multi output and maximum 200V DC
It would be even…
Part Number: PMP22650 Tool/software: Hi
i quiet like the design approach here, but the issue i am facing is that where to buy the magnetic parts in this design. Front End PFC coupled inductor and DC DC Transformer for CLLC stage both are little specialized…