Part Number: PMP22650 Hello folks,
Why two kind of voltage sensing required for grid (In mother board schematics)
1) TTPLPFC_VAC_N & TTPLPFC_VAC_P
2) TTPLPFC_VAC
are the net names, in the schematic.
Thanks and regards
Anoop kumar
Part Number: PMP22650 Hellow,
I'm trying to start PMP22650, but it doesn't work.
I tried to change the CLLLC_StartupState.CLLLC_StatupState_Enum of CCS, but an error prevents selection. Is this not reading the identifier of the source code? Could…
Part Number: PMP22650 Other Parts Discussed in Thread: TIDM-02013 Hi,
I am struggling to find VI-20174A, FRM-DOC-15 and RLTI-1379 to name a few, when trying to produce the PMP22650 reference design.
I found these components on the BoM for the TIDM-02013 reference…
Part Number: PMP22650 Hello
if we use SiC instead of GaN, the body diode of Fast leg and Slow leg can b utilized for preacharging the bulk cap of Totempole. The D10 (TS40P05GHD2G) given in the schematic is not mandatorry. ryt ??
Regards
Anoop kumar…
Hi Darwin,
If its possible will be great that you provide me the manufactures files of the magnetics. I mean dimension, wires, turns, materials all that stuff and in that manner we can provide to our local manufacture to construct the magntics.
Do you…
Part Number: PMP22650 Hellow,
We are planning to run the PMP22650 at 1-2kW output power as a trial.
When operating the PMP22650 with an output power of 1-2 kW, is it necessary to operate differently than when operating at ~7.4 kW?
I'm thinking of using…
PMP22650 is designed with an HSEC connector at its core. for this reason both TMDSCNCD 28388D and TMDSCNCD280039C can be used to control it. The code for TMDSCNCD280039C is provided in the digital power SDK on ti.com.
The daughter card is a fully programmable…
Part Number: PMP22650 Hello,
We plan to assemble the PMP22650 reference design and while looking at the BOM, we found out that the following 3 parts have a very long lead time:
MPN: RLTI-1373 (Rogowski Coil with Fly Leads-PMP22650E2)
MPN: RLTI-1371 …