Part Number: PMP40379 Other Parts Discussed in Thread: NE5532 , LM833 , UCC256302 , LM5161 , LM5160A Hello,
I am working off the PMP40379 reference design.
Can you all suggest alternatives to 750343844 Transformer, 220 uH, TH?
We are looking for a cost ef…
Part Number: PMP40379 Other Parts Discussed in Thread: PMP20195 , PMP10215 Hello,
I am developing 500W power supply.
I am looking for the PCB CAD file, the ASCII files for this reference design.
Please kindly point me to the URL. Thank you.
Best Regards…
Part Number: PMP40379
Hello
I have a major question in refrence to the above refrence design.
When loading one rail of the SMPS output as below, what is the resulting voltages?
Example 1:
Loading the +42V rail with 6A (+ & 0) not loading the -42V…
Part Number: PMP40379 I am wanting to make the PMP40379 power supply for a project; this is the first larger project I have put together. I have found all of the parts in the build of materials but I cannot find this transformer. I was wondering how I…
Hi Edward,
It is possible. Please have a look at this reference design PMP40379 . It shows the older UCC256302 uses without a PFC front-end.
I hope this answers your question.
Hi Sathish,
You can use UCC256404 without pfc input.
Please refer the single stage LLC without pfc reference design ( PMP40379 Schematic ). You can modify this design according to your requirement. Here when the AC input is between 100-120V, switch at the…
Hi Cihangir,
Please find the responses below:
1. The max IFB current for UCC256403 is 182uA. Please see the screen shot of the datasheet below.
2,3 . You are correct. You can not exceed the maximum cathode to anode voltage of the regulator. That's the…
Part Number: UCC256402 Other Parts Discussed in Thread: PMP40379 , UCC256302 , , TL431 , UCC28064A , PMP21366 , UCC24624 , PMP40281 , UCC256301 Hello,
I am working of the PMP40379 reference design, same specification, audio application.
Kindly recommend and or…
Part Number: UCC28019 Other Parts Discussed in Thread: , UCC256302 , UCC256402 , PMP40379 , TPA3255 , , UCC28180 , UCC28056 , TIDA-010081 , UCC25640 Dear Sir/Ms.
May I request UCC28019AEVM schematic and layout source file include BOM for evaluation and design…
Hi Austin,
Does the negative rail also need to support up to 10A load?
Could you also share what is the application? Something we have done before for audio loads that are 180° out of phase is reference the feedback circuitry to the negative rail and…