Part Number: PMP40766 Other Parts Discussed in Thread: UCC256403 Tool/software: Hi,
During no-load operation, the output voltage is 71.4V. When a 30-ohm pure resistive load is applied, the circuit operates normally with the red indicator light on, the…
Part Number: UCC256403 Other Parts Discussed in Thread: PMP40766 , , TINA-TI Tool/software: Dear TI Team,
I am developing an LLC DC/DC converter for a battery charger, referring to the PMP40766 reference design. Since this is my first LLC design, I…
Part Number: PMP40766 Tool/software: Hi,
In the PFC circuit, can the 47-ohm resistor RF1 under C11 be replaced with an ordinary resistor? If not, can I directly short it to test the voltage across C11? Now, when the input voltage is 220VAC, the voltage…
Part Number: PMP40766 Other Parts Discussed in Thread: AM2431 Hi ,
We want to make design up to 84V , 10A output. So what are the components and parameters need to change into the exciting reference design.
Regards,
Nilesh
Part Number: PMP40766 Tool/software: Hello,
Would like to ask regarding the use of MCU for CC/CV control. How would the implementation be like? Is there a need of additional circuit for Vbias/IREF signals in order to change the voltage/current setpoint…
Part Number: PMP40766 Tool/software: Hi ,
Generally speaking, the dotted terminals (polarity markings) of the transformer in a half-bridge LLC converter are typically the same for both primary and secondary windings. However, in this specific design…
Part Number: PMP40766 Other Parts Discussed in Thread: UCC256403 Tool/software: Hi,
We are working on 1200W EV charger (58V, 20A).
We have chosen UCC28180DR for PFC & UCC256403 for LLC, also we are referring PMP40766 reference design.
In this design…
Part Number: PMP40766 Tool/software: HI,
When the LLC circuit is in constant voltage control mode, Vout = 71.4V. When the current decreases to 0.7A, the non-inverting input terminal of U6A should be 0.175V through calculation. The inverting input terminal…
Part Number: PMP40766 Other Parts Discussed in Thread: TL103W Can anyone explain how the CC and CV mode works in the reference design?
At Vbias point we get a voltage of 2.5V approx. And Vref is 7.3V aprrox.
How this opamp U7A works in CV mode?