Part Number: PMP41106 Hello,
I believe there is an issue with the design files for the PMP41106 reference design.
I downloaded the file TIDCGR1.zip, which is listed on the TI website as the Gerber package. However, the ZIP only contains the following…
Part Number: PMP41106 Tool/software: Hello, I'm developing a battery charger based on the PMP41106 application note. Due to the UCC255603 being unavailable for mass production, I'm using the UCC256601. I have the same configuration as the schematic, but…
Part Number: PMP41106 Other Parts Discussed in Thread: UCC256403 , PMP40766 Tool/software: Hi,
My customer is currently considering the development of a 500W, 48V battery charger (output voltage: 55V to 40V, output current: 10A, CC/CV control).
During…
Part Number: PMP41106 Tool/software: Request for Schematic Review – 25.2V, 20A Charger Design (Based on PMP41106)
Hello,
We are developing a 25.2V, 20A battery charger using the PMP41106 reference design . Our design is based on the 48V, 10A schematic…
Part Number: UCC25660 Other Parts Discussed in Thread: PMP41106 Tool/software: Hello, I'm design a battery charger following the application example PMP41106 but with a bit different specifications.
I'm using a CISNS of 150pF and a RISNS of 130Ohms…
Part Number: PMP41106 Tool/software: Hello, can you share the specifications of the resonant inductor and the transformer? For the inductor, it would be nice to know what inductance and core type you are using. For the transformer, it would be nice to…
Part Number: PMP41106 Other Parts Discussed in Thread: TL103W Tool/software: Hello, I've followed the PMP41106 to design a battery charger with 52V output. But when I powered up it seems to be triggering OLP even if there is no load.
Reviewing the schematics…
Part Number: UCC28180 Other Parts Discussed in Thread: PMP41106 Tool/software: I'm developing a 25.2V, 20A charger using the PMP41106 reference design. The design includes a PFC, LLC, and flyback stage. I have developed a schematic and PCB, and I would…
Part Number: UCC28910 Other Parts Discussed in Thread: PMP41106 , Tool/software: I'm developing a 25.2V, 20A charger using the PMP41106 reference design. The design includes a PFC, LLC, and flyback stage. I have developed a schematic and PCB, and I would…
Part Number: UCC25660 Other Parts Discussed in Thread: PMP41106 Hi,
With respect to PMP41106 refernce design, Can I replace UCC256601 with UCC256603?
Because UCC256603DDBR not available.