Part Number: PMP4636 Hi,
I require a Led power supply design with the following specs: 230Vac Input, Vnom = 51V, I = 2.2A.
I came across PMP4636, this along with a DC/DC buck converter (maybe a LM3409HV) will be perfect. Is the PMP4636 available as an…
Hi Florian,
I checked PMP4636 and have following questions.
1. Is it dimmable supply? If yes, using what method (triac/Analog/PWM)?
2. If answer to 1 is Yes, which pin is dimming input?
3. If it is PWM, what should be minimum voltage of PWM wave?
4. Is…
Edin -
there are a number of power supply designs available in our PowerLab reference design library.
One possibility which meets your criteria is PMP4636 . Please have a look at the database as there could be other appropriate choices.
Another option…