Other Parts Discussed in Thread: PMP3199 , TPS5124 Dear Sir,
wanted to increase the current rating to 48 to 50 amps, require your help and support for the necessary changes. can only addinding an additional mosfet will do along with the transformer. this…
Do you have, or where can I get, information on the transformer for PMP5967; I assume it is custom, are the specifications available, and how were they created?
Thanks,
~Leonard
Hi Eric Faraci,
thank you for the explanation.
i have two problems:
1) in the case of UCC25600, in the PMP5967 reference design, the input/output voltage ratio is approximately 32 ( ie 380/12 ). the performance of the design seems high.
2) in your answer…
Other Parts Discussed in Thread: UCC28600 , PMP3199 , UCC28950EVM-442 Dear Sir,
We are in the process of designing and manufacturing server SMPS, The gerber file for the EVM will certianly fastern the process, we have already decided to us the PMP3199.1-TPS5124…
Hello Ti Support Forum,
I managed to find my answer hidden within a Ti drawing number PMP5967 Rev C found here http://www.ti.com/lit/pdf/slur470 . Looks like I can use a TPS71550DCK linear regulator from the 12Vout to supply 5Vcc to the UCC24610.
This…
400VDCin, 12V@460W, LLC with Synchronous Rectifiers.
http://www.ti.com/tool/pmp5967#1
Also this product was You should try to set the input AC220V(50/60Hz Single phase) . This device allows you to adjust the value of the current should try . Device tries…
Hello Betty,
Unfortunately, I was unable to find a schematic example for you of UCC256301 for 850V DC. But may I suggest two possible solutions:
1. UCC256303: HV startup is disabled so you would not have to worry about it. The high voltage path components…