Hi Anthony
in PMP6703, why need to use double mosfet for each side. Mosfet BSC059N04 has rating current of 73A, why need 2 pcs
regards
Tran Hung
Viettel Group
Part Number: LM5145EVM-HD-20A Hello.
We are looking for power supply solution with parameters as followed: - Topology - buck - Vin = up to 36V - Vout = 13V - Iout = 20A
The main requirement is the availability of development board or EVM, because we have…
Hi Anthony
Thanks for your reply PMP6703 using minimum switching frequency of 100khz
is there any problem if it runs with 300kHz?
in addition, my app run at 15A in 1 second then keep staying at 100mA.
regards
Hi Akshay,
I recommend looking at PMP6703 then following the design/layout very closely with necessary adjustments in the ratings of the output capacitors and the compensation. The equations in the datasheet can be used to choose the values for the inductor…