Hey Ben,
Since that is beyond .bt spec limit, they have to choose between a few options.
1. They could use 2x TPS2372 with a single RJ45 port in Beyond BT application
2. They could do a dual PD and dual DCDC that combine at the output to deliver greater…
Hello Vijay,
From your requirements you want dual output (12V and 24V). A buck regulator will only provide a single output. Also, Webench is only good for single output designs. So, based on the power requirements one possibility is the forward converter…
Part Number: PMP9656 Other Parts Discussed in Thread: PMP8861 Hi team,
My customer followed the PMP9656 and successfully built a design for 48V to 12/20A applications. Now they have a new project, hoping to extend the input voltage range to 24V-48V, but…
Hello Yue Tang,
The UCC2897A is a similar part to the LM5025A
PMP8861 reference design is an 18-72VDC Input, 12V/120W Active Clamp Forward Reference Design.
http://www.ti.com/tool/PMP8861
Regards
John
The image you have shared are for 12W supply, we are designing for 120W supply with below specifications:
input 18V to 80VDC & output 24V, 5A
we wish to have the 120W transformer information as shared by you for 12W supply. we are unable to get this…