Part Number: PMP9256 Other Parts Discussed in Thread: LM5122 I have tried to use the equations in the LM5122 datasheet to calculate the inductance, peak current & RMS Current, but the value is in negative for the below specification. Please share the…
Part Number: PMP9256 Tool/software: Hello. I'm developing an isolated DC-DC converter based on the PMP9256, but the output voltage ripple is too high.
The schematic structure was designed to match, and the PCB was built with two layers. I've attached…
Part Number: PMP9256 Dear sir,
We have completed successfully our proto unit development of qty 2no.s of DC DC converters by following the PMP9256..
These two units are working from 9V to more than 40V DC input voltages with output current of 5Amp…
Hi Maria,
It looks like you are interested in designing a differential mode LC filter. You might find this app note helpful. This design calculator may also be useful.
All the best,
Pradeep
Part Number: PMP9256 1. We designed the board as per available gerber in the application note PMP9256.
2. The design includes some of DNP (Do Not Place) components and the PCB is provided with mounting locations for these components also. As per the…
Part Number: PMP9256 Hello
I am working on a 12V-60V to 13V 5A flyback design for a traineeship in Rockwell Collins France and I am very interested in the PMP9256 evaluation board. Unfortunately this part is not avalable yet on the website...
Is there…
Part Number: PMP9256 Hi team,
From BOM, it seems there are some typos on CSB2 & CSB3 descriptions. Could you please advise the type and voltage rating for the ceramic capacitors? Thanks!
Best regards, Sam Ting
Part Number: PMP9256 hi,
Testing instruments:Spectrum analyzer-agilent E4402B, Resistance loader-IT8512
Input voltage:24V, Output 12V@2A
We tested the radiation at various locations on the PMP9256 board with a near-field probe and recorded the…
Part Number: PMP9256 Dear Sir,
The output Ripple is around 160 to 140 mV with 20 MHZ band limited Scope.
Is there any suggested ripple suppression filter or any other circuit modification such that the ripple can be reduced to a level of 10mV.
Part Number: PMP9256 Hi All
We are interested to use this power supply design for our industrial standard application.
Our design requirements are mentioned below.
Compact design, 24V Input, 12V Output @ 5Amps (steady-state operating current)…