Hello
looking for the problem of this post i tried the verbose of the syslink module in EZSDK 5_05_02_00 (running the sw on the EVM8168). I found this problems. Could someone help me to understand and correct this issue? I see also that if you try to…
Hi Dwarkesh,
Please find attached logs dmesg,usb analyzer log of AM572x and Linux PC for UAC1.
2055.am572x_dmesg_04sep2017_uac1.txt 0763.Linux_PC_dmesg_04Sep2017_uac1.txt
Set Interface is getting Stalled in PC and not received in gadget(AM572x…
Hi,
Are you referring to this document?
https://www.ti.com/lit/ug/tidueo2a/tidueo2a.pdf
TIDA01614 Multiparameter Front-End Reference Design for Vital Signs Patient Monitor.pdf
Yes, ADS1298EVM does not have the TVS diode.
It's not necessary…
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAPL138 Hello,
I am using OMAPL138 SoC on my hardware board and after running for few days I get an error every 24 hours as per the message file in the /var/log/message (attached)
Any idea…
Zhongyuan Guo ,
Good day!.
These CSL API functions are part of the SDK ( Software development KIT) .
SDKs are developed for the EVM boards with C6657 processor.
EVM boards are meant to demonstrate the features, capabilities of the TI processor…
Other Parts Discussed in Thread: OMAP-L138 Tool/software: Code Composer Studio Hello
I am working with LCDK-Omapl18 board
Few days back I installed ti-processor-sdk-rtos-omapl138-lcdk, in CCS10 . And I have successfully installed the PDK example for…
Hi,
More or less, the performance would be same at both 868MHz and 915MHz bands.
Please refer to the App Note SWRA588.
Attached is the App note for your ready reference.
swra588b.pdf
Thanks,
PM
Hi John,
I managed to successfully flash MLO, u-boot.img, uImage and ubi.img to NAND and then boot them entirely from NAND by following the steps below.
I'm using Ubuntu 12.04 with ti-sdk-am335x-evm-05.06.00.00 and MTD-UTILS v1.5.
# cd ti-sdk…
Other Parts Discussed in Thread: TPS65910 Hi,
we are using AM335x EVM , with in that i have tried to boot using NAND flash with ubifs flash file system, but it shows ECC error, i am using ti-sdk 7.0 and i have also checked both the u-boot and kernels…