Other Parts Discussed in Thread: DM3730 , ADS7846 Hi,
I am trying to boot the EVM using the " dvsdk_dm3730-evm_04_03_00_06_setuplinux ". But the board stops at
"[ 4.806610] Waiting for root device /dev/mmcblk0p2..."
I want to use the Board for the…
I just downloaded the new release of Texas' SDK that comes with the Linux 3.2.0-psp04.06.00.11.
After a few changes in the Kernel configuration via make menuconfig to use the same options I use in the older version I have (psp04.06.00.08), the uImage…
sdk version :ti-processor-sdk-rtos-j721e-evm-08_00_00_12
full boot and vision apps init log is as follows:
Starting kernel ...
[ 0.000000] cma: Failed to reserve 512 MiB
[ 0.047433] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0…
Part Number: LAUNCHXL-CC2640R2 Hi,
im working with the cc2640r2 LP and simple broadcaster example. My broadcaster goes into shutdown after recieving a scan request from my observer.
I have measured the current of my broadcaster from start to shutdown…
Part Number: AM5728 Other Parts Discussed in Thread: BEAGLEBOARD-X15 , PMP , DRA752 , TMP102 Tool/software: Linux Hi,
we are developing a custom board based on AM5728 ( using SOM module from Phytec).
Initially we are able to modify the TI SDK sources…
Other Parts Discussed in Thread: TVP7002 , THS7353 , TVP5146 , THS7303 We currently are working on a custom board we built which uses the dm368 for encoding. We have also built a custom input board. We used the Leopardboard with the TVP7002 as a development…
Part Number: TMDSICE3359 Other Parts Discussed in Thread: AM3359
AM3359 Industrial Communications Engine TMDSICE3359. SDK 3.02.00.05. Linux RT (default by create-sdcard.sh)
There are complaints about the bug. From time to time an error on commands…
Other Parts Discussed in Thread: DM3730 , ADS7846 , TVP5146M2 Hello,
I'm trying to boot DM3730 via minicom. First, I opened minicom, then turn the power on. It starts to boot, but then at some point it stops booting. This is what I see on the screen…
Part Number: AM3359
When we tested on AM335x EVMSK, we found that the number of drivers loaded at each startup was different.
The two startup logs are as follows:
Fullscreen
47_driver.txt
Download
U-Boot SPL 2018.01-g9d984f4548…
Part Number: LINUXSDK-OMAPL138 Other Parts Discussed in Thread: TMDSLCDK138 , OMAPL138 , OMAP-L138 Hi TI experts,
We are using:
1. TMDSLCDK138 board revision A7A. 2. PROCESSOR-SDK-LINUX-OMAPL138 version 06_00_00_07. 3. Custom device tree 6076.device_tree…