Part Number: PROCESSOR-SDK-AM62X Other Parts Discussed in Thread: AM625
Hi,
Actually we are working on AM625 Processor in which i wanted to study about R5F processor how to works or can we program it if possible how to program it ? how to use that processor…
Part Number: PROCESSOR-SDK-J721S2 KB,
I am looking into the main domain reset changes to fix the MSMC/ECC interaction and don't see the changes right off.
Not using the sciclient/sciserver model, so just need the explicit register resetting steps…
Part Number: PROCESSOR-SDK-AM62X Hi
May I have question about AM62x Debian SDK v9.02?
I want to install wine for use windows application test.
I tryed following this manual,
https://wiki.debian.org/Wine
I installed both wine64 and wine32.
Question 1 …
Hello Krunal,
Thanks for your information.
I understand it.
Do you mean that X11 was support only SDK v4, that is supporting older processor as AM335x, AM18xx?
In upper version of SDKv5, X11 is not supported, but SDK user guide had been continue to be…
Part Number: PROCESSOR-SDK-AM62X Other Parts Discussed in Thread: SK-AM62B Hi
In my customer's enviorment(SK-AM62B, using Debian SDK), there is issue about maybe from OpenGL.
Question 1
Is there anything to OpenGL API guide for Debian SDK?
Question…
Part Number: PROCESSOR-SDK-AM57X When the newe processor sdk (based on Kirkstone branch of Yocto) gets released, how will the users (e.g. me) be informed? Where can I notice the announcement?
Part Number: PROCESSOR-SDK-AM335X Hi
I want to build the kernel source code (am555x board).
I have clone linux-5.4.y branch.
When i tried this command facing issues.
make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabihf- tisdk_am335x-evm_defconfig scripts…
Part Number: PROCESSOR-SDK-AM64X Hi,
I am having some issues with "Flashing Linux to eMMC" Flash Linux to eMMC (ti.com)
I believe I am following the instructions correctly. The only minor issue is the renaming of the file u-boot-am64xx-evm.img…