Part Number: PSIEVM I was testing the PSIEVM PA045B output with the Precision Signal Injector tool, and I noticed that I was unable to change the offset. I verified with the user guide that the SE_VCM jumper JP4 was connected to VCM and the DIF_VCM jumper…
Part Number: PSIEVM I would like to struct automatical measurement system by using this "PSIEVM" software by python
I have tried to make python code by using library of "pyautogui" and debuged.
But PSIEVM software could not response…
Part Number: PSIEVM Hi,
Is this possible to automate the use of the PSIEVM?
- via the PSIEVM software by passing arguments or file contening amp, offset, frequency, ...?
- others solutions?
Thanks
Part Number: PSIEVM For the PSIEVM is it able to output DC - non sinusoidal signals (i.e. 0 Hz ) ?
What is the smallest possible differential voltage Vpp the PSIEVM output ?
What is the resolution of the voltage Vpp the PSIEVM output ? i.e. what is the smallest…
Part Number: ADS8900BEVM-PDK Other Parts Discussed in Thread: ADS8900B Hi Team,
My customer is working with the ADS8900B EVM and is now doing evaluations and ran into a few questions. With the PSI-EVM, will it only offer a 2-kHz input signal? He's noticed…
Cedrick,
The implementation on the controlCARD supports what the customer wants to do, in terms of both available ADC channels as well as the reference network. From above differential input comment, they will be using the ADC in 16-bit mode. At this…
Hi Devin
Thanks your so much detail advice.
I have apply the PSIEVM and DIP-ADAPTER-EVM according your recommend, will setup test platform to re-verify ADC performance after receive kits.
Since kit setup still need wait some time, if you already have been…
Part Number: ADS8320 Other Parts Discussed in Thread: REF3025 , PSIEVM , LMP7716 , OPA354 Hi, All:
We are planning to use ADS8320 in our project, and we bought an ADS8320EVM and are evaluating the baisc features.
Now we met an issue of SNR.
We tested your…
Danilo,
I would suggest the customer take a look at this application note, it will help them understand the driver circuit/settings they can use to optimize the ADC performance https://www.ti.com/lit/spract6 . Especially if they are evaluating 16-bit mode…