Part Number: ADS8900BEVM-PDK Other Parts Discussed in Thread: PSIEVM , ADS8900B Hello,
We want to evaluate ADS8900BEVM-PDK while having the following questions
1, We can not find a link at TI official site to purchase PSIEVM, can you direct?
2, when evaluate…
Hi Gandhali,
The 50 ohm resistors are there to function as termination resistors. This is a pretty normal way to source in a voltage from a function generator (see the below link). However, if you want, you can remove or replace the termination resistors…
Hi Taeyeong,
Is the sampling coherent or are you using a windowing function? If you are using a windowing function, you may need to center the signal before passing it to the windowing function (so that the mean sampled value is 0). Note that even after…
Hi Willy,
After you input the value for amplitude(Vpp) or Offset every time, you should click "Set" button to execute your change.
On PSI board, when you want to create a SE signal with filters, the jumpers position should be: JP1=Filt, JP3…