Part Number: PTD08A006W Hello,
We would need to have the STEP file of PTD08A006W for the mechanical check. Can you provide it, please?
Thanks and Regards,
Alfonso
Other Parts Discussed in Thread: UCD9248 Hi,
There was a question about the calibration of current sensed by the UCD9248 and how it relates to the output voltage. When the current is calibrated for a specific voltage, the reading from the UCD9248…
Other Parts Discussed in Thread: PTD08A006W We have a design with four ptd08a006w providing four different supplies. The four ptd08a006w share one inhibit line that is pulled-up via a 10kΩ resistor to 3.3V (generated by the controlling UCD). These are…
Other Parts Discussed in Thread: UCD9240 , PTD08A006W , UCD9248 , UCD7230A , UCD9224 We have several similar designs using a UCD9240 in a system driving either three or four PTD08A006W to provide multiple (single phase) rails. These rails are relatively…
Other Parts Discussed in Thread: UCD9240 , PTD08A006W We have a design with an UCD9240 and three single-phase power rails using the PTD08A006W. We are having some trouble debugging start-up problems as the system seems to log faults on all the rails during…
Other Parts Discussed in Thread: UCD9222 , UCD9240 , LM25056 , PTD08A006W , UCD74106 Hello everyone,
as I am trying to use the Fusion Digital Power Designer for power measurements (Voltage and current). It is planned to use a UCD9240 or UCD9222 as…
Other Parts Discussed in Thread: UCD9240 , PTD08A006W We have a design with an UCD9240 and three single-phase power rails. We have found that after the system warms-up (UCD9240 case temperature with a thermocouple attached ~65°C) we get semi-random rail…
I did not receive any emails from you having the latest code but I did download from the link you send earlier here is the version I'm using
Right now I have newly made boards with brand new parts on them and since I'm unable to load my xml file not…
1. Increasing the rise time in the rail configuration interface is effective; setting it to 48ms or 60ms both work, as shown in the figure below.The problem is that when setting it below 30ms, it fails to take effect.
2. Increasing or decreasing…
Other Parts Discussed in Thread: PTD08A006W , UCD9240 , PTD08A010W Hi
Does anybody know if I can just directly connect IOUT of the PTD modules (e.g. PTD08A010W or PTD08A006W) to UCD9240. The simple schematic in the datasheet shows a direct connection…