Part Number: PTD08D210W Hi,
From the datasheet of PTD08D210WAC, its maximum operating temperature is 85C. Could you please let me know what is the maximum junction temperature supposed to be for this module? Thanks.
Regards,
Bob Mao
Hi Maxime,
Do the calibrations steps I sent you work? I used the same EVM when I sent you those steps in the last post, so I don't believe it is an issue with the UCD or EVM. I am not sure if the PTD08D210W is behaving as it should because the voltage…
Part Number: PTD08D210W Other Parts Discussed in Thread: UCD7242 , UCD9248 Hi,
We have used 4 PTD080D210W power modules in our design in which one of the module is programmed to output 1V & 1.8V. In this 1.8V section failed when powering the board and when…
Part Number: PTD08D210W Hi,
We have been using four PTD08D210W modules following the eval board of XC7Z020. On the board, one of the module's temperatures crosses more than 70 °C. The only difference between the modules in the XC7Z020 Eval board and…
Hi Jeevan,
I do not know the Aquanox A4727 cleaning solution and need to study this.
But have you ruled out presence of chemicals/gases in the installed area?
We have never encountered this issue before.
Regards,
Yitzhak
Part Number: PTD08D210W Hi,
Good Day.
On one of customer's legacy PCBs, they use a combination of PTD08D210WACT and UCD9248PFC. They build 11 PCBs recently but 2 of them have a 'FLT' fault on one rail (see System Monitor.PNG attached),
the…
Part Number: PTD08D210W Hi,
I am using PTD08D210W with UCD9248PFC. I am not able to understand the pin descriptions of PWMA, SRE & FF. Can you give me a detailed description and the function of the pins?
Thankyou!
Part Number: PTD08D210W Hi team, The inductor inside the module has been damaged. The inductor is probably cracked due to heat generated from the inside. Please tell me the reason why the inductor breaks? And, can I ask what name is the inductor in a module…
Part Number: PTD08D210W Dear TI Team
When I checked the data sheet of PTD08D210W, there is no description of recommended land pattern or recommended layout. If you have any information on recommended land patterns and recommended layouts for PTD08D210W…