Part Number: PTH08T240W Hi team,
When use 12V input, 5V output, the output current can only reach 1A. They need about 10A output current. Could you help to solve this problem? Thanks.
Below is the schematic:
Part Number: PTH08T240W Dear Community members,
We're building power supply for FPGA and wish to use the PTH08T240W in our design but as there's no simulation model available we're not able to take it further.
Please help so we can move forward…
Part Number: PTH08T240W
Hi Team,
For PTH08T240W, o ur customer would like to know if the value of the capacitors must include DC bias derating (eg. is 5 x 47uF adequate for the 220uF input?)
Regards,
Danilo
Part Number: PTH08T240W Other Parts Discussed in Thread: PTH05T210W Hi Team, What is the maximum junction temperature for PTH08T240W and PTH05T210W buck modules? Kind Regards, Jejomar
Part Number: PTH08T240W Other Parts Discussed in Thread: PTH08T241W Hi,
We have a problem with PTH08T240W. According to the datasheet, when RTT is short (0 Ohm), we need a high output capacitance (~2000uF). If we are using 2x100uF with ESR 5mOhm each…
Part Number: PTH08T240W Hi Team
please provide details for below issue.
1) What is the minimum spec for component height after running reflow as per picture below ?
2) What is the recommended tooling depth if to hold the component to prevent from component…
Part Number: PTH08T240W Hi E2E,
Our customer is requesting the PTH08T240WAD and PTH08T230WAD thermal resistance information.
Thank you in advance for the help.
Regards, Carlo
Part Number: PTH08T240W Hi:
The normal output of PTH08T240W is 1.2V, but due to the short circuit of 10uF load capacitor at the output end, after replacing the new load capacitor, PTH08T240W can output 1.2V normally. But after a period of operation…
Part Number: PTH08T240W Other Parts Discussed in Thread: LM3880 I want an LM3880 power sequencer to control PTH08T240Ws connecting FLAG pins to inhibit pins directly. Referring to the datasheet of LM3880, FLAG pins are limited to MAX. 6.0V. But I cannot…
Part Number: PTH08T240W Other Parts Discussed in Thread: TPS563200 Hello,
Here is a query from my customer-
In our current design, we have one board sourcing 3.3V from a TPS563200DDCR regulator. A second board makes 3.3V from a PTH08T240W but then shorts…