Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: PTH08T240W I'm using a PTH08T240W on a 125MSPS ADC Board to power FPGA and other components.
Therefore I need preferably less ripple at power rails to get a clean FFT spectrum from ADC data.
Datasheet states a Vo rippl…
Other Parts Discussed in Thread: PTH08T240W We intend to use PTH08T240W, 10 A, 4.5V to 14 N INPUT, NON_ISOLATED, WIDE_OUTPUT, ADJUSTABLE POWER as programmable Power Supply for our NAND Test System.
The input is 12 V. The Output we need to be adjustable…
Other Parts Discussed in Thread: PTH08T240W , PTH05T210W Hi,
I am using PTH08T240W in parallel with another TI module (PTH05T210W ) but I only want one or the other to drive voltage into my 1.0V rail. We are using the inhibit pin in PTH08T240W to turn off…
Other Parts Discussed in Thread: PTH08T240W Sir:
I use pth08t240w in my board, and the sechmetic is in PIC(1). In my design, I use the TurboTrans Technology, and I choose the input capacitor Ci and output capacitor as follow:
type
Rated Volt
…
Part Number: LMZ31707 Other Parts Discussed in Thread: LMZ31710 , , TPS84A20 , PTH08T241W , PTH08T240W , PTD08D210W , PTD08A210W , LMZ22010 , TPS542A52 , TPS56C230 , TPS542A50 , TPS54A24 , TPS53319 , TPS51397A Hi,
We have the footprint for LMZ31707 or LMZ31710 designed…
Other Parts Discussed in Thread: PTH08T240W Hello,
We have 4 pth08t240w in our last board. 2 work, 2 don't (output voltage is down) They are practical copies of each other and all the input signals, feedback and senses seem to be as they should. The layout…
Hello Kent,
TPS84A20 is 100% compatible with LMZ31710.
You may also want to consider LMZ22010 , LMZ12010 , PTH08T241W , PTH08T240W .
I am not an expert in supply chain issues, so I will refrain from trying to explain the reason for the shortage.
Happy holidays…
Other Parts Discussed in Thread: PTH08T240W , UCC383 I need to get a high quality 5.0volts from 12volts power supply. The ripple should be controlled below 1mV. So, I want some expert advice.
The power supply structure I designed is showed below:
…
Other Parts Discussed in Thread: PTH08T240W Hello,
I have a design that requires 20 SFP optical transceivers (3.3V). The recommended power circuit requires 2 10uf caps per SFP module. That would be
40 10uf caps. Using ceramics with an ESR of 2milliohm…