Part Number: PTH08T260W Hello,
We are using PTH08T260WAZ power module in our design.
Unfortunately, the inductor on one of the boards has been damaged (photo below). We would like to avoid heating the entire board during a full module replacement…
Part Number: PTH08T260W Other Parts Discussed in Thread: TPS82130 , TPS82130EVM-720 Dear TI team,
We are developing a new design and we have chosen the PTH08T260W Power Module to manage the energy. We have searched the recommended layout in the website…
Part Number: PTH08T260W I want to know the date of manufacture of the product and how long it is going to be active.
In the sustainability column, you have mentioned EOL should be there in the material content tool but there is no any information about…
Other Parts Discussed in Thread: PTH08T260W Hello,
there's no absolute maximum rating for the input voltage specified in the datasheet of the PTH08T260W. What is the (transient) surge voltage allowed for this part?
Thanks!
Stefan
Other Parts Discussed in Thread: PTH08T260W Figure 5 of PTH08T260W datasheet has 8 verical subdivisions with 10 numbers beside; it is all misaligned. Is really the scale 6.25%/division starting at 50 or the printing is just messed up?
Thanks
Frederic…
Ankity:
PT5500 series is obsolete. PT5501
I recommend either PTH08T260WAx or LMZ31503 3 amp power modules.
The link to PTH08T260W is: http://www.ti.com/product/pth08t260w/samplebuy?keyMatch=pth08t260wad&tisearch=Search-EN
Tbhe link to LMZ31503…
Hi,
We spoke about my power application a few weeks back.
You had offered to give us our average power figures based on the voltage drop across the inductors.
Here are the modules we are using and the voltage drop across the inductors and…
Other Parts Discussed in Thread: PTH08T260W , PTH08T230W PTH08T260W is rated 3A. It can handle it at 85°C with convection only.
Its overcurrent threshold is 5.5A (typical, no min nor max stated).
We would load this module with up to 3.5A. I suspect…
Power quick search returns a lot of options:
LMZ10503
LMZ10503
Step-Down (Buck) Module
3
2.95
5.5
0.8
5
7PFM
3.75 | 1ku
TPS84320
4.5-V to 14.5-V Input, 3-A Synchronous Buck, Integrated Power Solution
Step-Down…