Part Number: PTH12050W Hi Team,
My customer is looking for the 3D/step file of PTH12050W
If available, can you provide the the file to us?
Thank you.
Regards, May
Part Number: PTH12050W If the POLA Regulator parts PTH12050WAD and PTH12050WAH are now mechanically and electrically "equivalent' why does TI still offer both options ? Producing both versions must have a cost associated. Is there an advantage to offering…
Part Number: PTH12050W Other Parts Discussed in Thread: LMZ31506 , LMZ31707 We use these Texas Instruments DC-DC converters in multiple designs. The PTH12050W is used to convert 12V down to both 3.3V and 1.2V.
Issue we are seeing is that the modules…
Part Number: PTH12050W The 12V supply voltage to this module has instances where it will temporarily go as high as 14V for a period of 1ms.
This spike is outside the maximum voltage for this part of 13.2V. Since it lasts for a small duration when it…
Part Number: PTH12050W Using PTH12050W with Vin = 12V, Vout set for 5V or 3.3V. Track pin is tied to VIN and Inhibit pin is unconnected.
When the module is powered up with zero load or near zero load, a glitch in the output is seen after about 18 ms…
Part Number: PTH12050W
Hi,
"SLTA055 - Februrary 2006" application report is a great app-note but, it's only apllying to single-phase, isn't? if so, is there a version for multi-phase e.g., 2 or 6 phases design?
Thanks,
Tim
Part Number: PTH12050W What is the difference between a PTH12050WAD and a PTH12050WAH and where in the data sheet does it spell this out?
What is the difference between a PTH12050WAS and a PTH12050WAST and a PTH12050WAZ and a PTH12050WAZT and where…
Other Parts Discussed in Thread: PTH12050W , PTH12060W I'm working on a power distribution design which is heavily based on previous generations in which I'm using the PTH12050W to generate one of the low current rails (<5A). I would like to add a feature…