Part Number: PTH12060W PTH 12060WAD Z532E. : Inhibit circuit 12 VDC vs 8VDC expected at Inhibit input?
I have a couple of older (2015 / 2016) field units that measure 12 VDC at the inhibit input of PTH12060WAD part #. They also have a Z532E marking following…
Part Number: PTH12060W Hello team,
I'm reaching out to confirm if this power module is exacly the same product with another manufacturer Artesyn Embedded Power.
I attached the datasheet here for reference.
pth12060_b0046d08b7.pdf
Part Number: PTH12060W s1.Track pin coneected to Vin(12V)
2.Inhibit Pin used for getting Vout
-> We used moee than 100 boards using PTH12060W but one of them shows different waveform with others.
When inhit(pin) is activated,Vout shows unstable for 20ms…
Part Number: PTH12060W Are there any issues or guidelines regarding conformal coating of the surface mount versions of the PTH12060W supply module (PTH12060WAZ/PTH12060WAZT)?
Part Number: PTH12060W Dears,
we are going to using PTH12060W Through-Hole module.
but i found there are 2 part number.
what is the different PTH12060WA D and PTH12060WA H
is there any different specificaion?
thanks.
Part Number: PTH12060W Hi
This is max. koh in WSSystem.
I have a question.
What is the differnce between PTH12060WAD and PTH12060WAH?
Please help me?
Thanks,
Max.
Part Number: PTH12060W Hello
I have a question about pin 8 of the PTH12060W.
According to the data sheet, if you do not use No.8 pin track, it is said to connect with Vin.
If nothing is connected to Open without connecting No.8 pin to Vin, will it affect…
Other Parts Discussed in Thread: PTH12060W There are ten standoffs on this assembly. What is the solder requirement for this type of standoff (standoff has a step in the leads or legs)?
There is a customer that wants a full solder fillet on the step end…
I am in the process of certification of a product and need the latest UL and EN60950 reports.
I currently have "165166-A15-UL-3-Final-2nd edition .pdf" and "EN60950 2nd edition PTHXXXXXE165166-A15-CB-4Certificate.pdf" Are they the latest?…