Part Number: PTN78060A Other Parts Discussed in Thread: TPS82130 Dear TI support team,
can you provide an MTBF or FIT value at a certain temperature for the PTN78060A?
Thanks a lot in advance!
PTN78060A questions:
Response
1. Start of Production(Release date/Start of selling Point) : YYYY-MM
Production and full release selling was April 2005
2. Discontinued or Not : Y or N No
3. End of Production/Expected EOL Point : YYYY-MM(If it was…
Other Parts Discussed in Thread: PTN78060A the three 4.7 uF capacitors C2 that are labeled 'Required' with the PTN - these are a little hard to get right now, and I'm wondering if I can use electrolytic capacitors in their place. we need to get our project…
Part Number: PTN78000A Other Parts Discussed in Thread: LMZ34002 , PTN78060A , PTN78020A , We are using PTN78000AAH in our power supply module, no stock available in the market. Kindly suggest us the alternate or equivalent.
PTN78060A internal resistors.pdf The Rset equation is derived from the internal resistor divider on the feedback of the internal error amplifier. See attached.
The PT5042A and PT78NR215H have an average input inrush current each of up to 5.5A .
One possible alternative is the PTN78060A series with a lower inrush current from a maximum input voltage of 15V. The 40V power source is has to be regulated down…
We are using the inverting version PTN78060A.
Can the inhibit pin be utilized?
What is the function of the other undocumented pin (3 or 5). Wondering if we can externally sync to a 691kHz signal.
Other Parts Discussed in Thread: PTN78060A Our product uses a PTN78000AAH voltage regulator module with a 24V input and a -15V output. I have discovered that the regulator is supplying approximately 0.75A continuously. The datasheet maximum output current…